AXIS#.PL.ERR

Description

AXIS#.PL.ERR is the position loop error when the axis is operating in position mode (AXIS#.OPMODE = 2). It is the difference between the commanded axis position and the measured position. If the axis is not operating in position mode, AXIS#.PL.ERR is set to 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

N/A

Data Type

Float

See Also

AXIS#.PL.FB
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
AXIS1.PL.ERR

60f4h

00h

Signed32

Position

-

Read only

Yes

AXIS2.PL.ERR

68f4h

00h

Signed32

Position

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.ERR

5901

170D

Signed32

Read Only

Position

AXIS2.PL.ERR

71437

1170

Signed32

Read Only

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.ERR

5901

Signed32

Read Only

Position

Related Topics

AXIS#.PL.ERRFTHRESH | AXIS#.PL.ERRWTHRESH

"Position Loop"